Hello,
In a project i want to use MAX3243 IC. In particular situation, MAX3243 is not powered, whereas RS232 signals are present (imposed by a RS232 peripheral).
So I have 2 questions:
Could we apply a RS232 level on RINx pin (RS232 line data input) when the IC is not powered (VCC=0).
When Vcc=0V, what is input impedance of RINx pin?
Thanks
Sylvain B