This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

SN75C3243: Question about ESD specification

Guru 12940 points

Part Number: SN75C3243

Customer is testing SN75C3243 for ESD rating, a few device were abnormal operation.

Please let me know about three points below.

①Is there ESD specification for the other than 15kV HBM? (DIN / DOUT rating, etc)

②Are DIN and DOUT should connect TVS diode?

③After ESD test, a few device are floating output, is this likely occur?

 

【Background】

・ESD test condition: 11kV / 0.5sec (×several times)

・Abnormal operation: After ESD test, DOUT is drop 0.8V~1.0V (normal is 5Vout)

・After ESD test, all DIN were no problem.

Best regards,

Satoshi

  • Hello Satoshi-san,

    This part is only specified for HBM ESD (up to 15 kV). TVS diodes could be used externally if you need to subject the part to higher-stress transients. This would more likely be on the RS-232 signals (which would interface externally) than the lower-voltage logic signals (which typically remain on the application PCB).

    Typically ESD failures result in short circuits or increased leakage rather than floating outputs, but it is possible for high-current stresses to cause units to have open-circuit failures (floating outputs).

    If you want to get a better understanding of the nature of the damage to these units you could request a failure analysis be performed by TI. Let me know if you need any explanation on how to go about this process.

    Regards,
    Max

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.