Hi Team,
I have two qestions as the following.
1)
The datasheet shows "Operating virtual junction temperature" is 150℃(MAX).
What does "Operating virtual" mean?
2)
Is MAX3232E-Q1 operable at Ta =95℃?
I heard it is possible case that Ta(ambient temperature) increases up to 95℃ for my customer's automotive application.
I understood max and min of ELECTRICAL CHARACTERISTICS show under –40 to 85℃ condition, however I would like to confirm above.
Your support would be appreciated.
Best Regards,
Yaita / Japan disty