This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MAX3232
Hi,
MAX3232 RθJC can reference to MAX3232E?
I can't find MAX3232 RθJC data from datasheet.
Thanks!
Jeff
Regards,
Michael Peffers
Industrial Interface Applications
Analog Wire: Get Connected
In reply to Michael Peffers:
Hi Michael,
I'm searching for MAX3232CPWR TSSOP 16PIN package, but if possible,
Could you please give me all 4 kind of package RθJC?
In reply to JeffYC Yang:
Hi Jeff,
Here is the thermal information for the D package:
Ambient Temperature 25
Result- Theta JA-High K 66.6
Result-Theta JC, top 32.4
Result-Theta JB 31.9
Result- Psi JT 8.4
Result- Psi JB 31.5
I am still waiting on the other packages and will respond when I have it. Also, I will see about updating the existing datasheet to include this information.
ok, if you get "MAX3232CPWR TSSOP 16PIN LF" thermal information, please let me know.
Sorry for the delay. Attached are the thermal metrics for all packages of the MAX3232 device. Please let me know what else you need?
MAX3232 Thermal Metrics.pdf
Is the MAX3232PW = MAX3232CPW?
I have no find MAX3232CPWR TSSOP 16PIN package in PDF file.
thanks!
The thermal parameters are the same for the C and I versions of the devices. SO the PW thermals for both C and I are:
Please let me know what other questions you have?
thanks for your information!