Other Parts Discussed in Thread: STRIKE
Hello,
Our customer use the MAX3232, have an issue of DOUT voltage.
The customer observe DOUT voltage as 1V. The DOUT1 voltage is 5V, it is no problem.
Only the DOUT2 voltage is 1V.
When RS232 cable disconnect, the voltage of the DOUT is 5V.
The customer use the MAX3232 at 3.3V and C1-C4 is 0.1uF. The customer change the capacitor
from 0.1uF to 0.47uF, it occur same issue.
Is this device damaged?
I attach the scope shot of V+/- voltage.
Best Regards,
Naoki Aoyama