Other Parts Discussed in Thread: MAX232
Hi,
I have a design in which the part MAX232 from MAXIM INTEGRATED was replaced by TRSF323ECDR to use 3.3V supply to IC.
Whoever changed the part kept the external capacitors:
C1=C2=2.2uF instead of 0.1uF.
And C3=C4=10uF instead of 0.1uF.
Communication with RS-232 is working.
Is there any danger to the IC in the long run when using the above values instead of typical values?
Thanks,
Yossi