This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TRS213: different between ADM213 and TRS213

Part Number: TRS213

Hi Sirs,

We would like use TRS213 to replace ADM213EARSZ/SSOP.

But we saw there only show P on TI cross reference, not show "S" 

  • P: TI device has the SAME FUNCTIONALITY as the competitors device, but is not pinout compatible and may not be parametrically equivalent.

May i know what different between them? have any risk if we use TRS213 to replace ADM213?

Thanks!!

  • Shu-Cheng,
    A few parameters have minor difference between these two devices. For example, TRS213 has a little more power consumption of no load normal operation and shutdown. Other than that, they both offer same pin-out and same package. It should be OK to replace ADM213 by TRS213.
    Regards,
    Hao