Hi,
We are making a product that has the controller and communication modules. Controller module will be installed in a pit under the ground. Communication module will be installed over the ground. Both these modules are exposed to external harsh environment conditions. The distance between controller and communication module will be 10metre (max), and connected through a cable. The basic interface/protocol will be UART between these two modules. Due to harsh environment, we want to use a suitable cable interface that can sustain hardships posed by external environment.
With the above consideration, I have started pursuing the widely used and popular interface RS232. But I am not sure whether pursuing RS232 is the right choice. The supply voltage in both the above modules is 3.0V, and the number of drivers & receivers are 2 each. I have few doubts as below. Kindly clarify the same.
- Is RS232 the right interface for my above needs? If not, can you suggest any other suitable interface?
- Since my supply voltage requirement is 3V, I was considering the IC with its supply voltage range beyond 3V. For example, I want the IC with the range of 2.0V to 3.6V, where-in 3V falls in between. Somehow, I could not get any IC matching my above requirement. However I started looking into TRS3122E, but it also does not meet my above requirement. Can you suggest any suitable IC meeting my above requirement?
Regards,
Vikas Chandra Rao.