Hi Sirs,
Sorry to bother you.
We have some questions on TRS3122E.
1. Please help check our function block is OK ??
2 Does TRS3122ERGER have support level shift function on 1.8V to 3.3V?? If yes, we could remove up board level shift IC.
3. Do we need add one more TRS3122ERGER on down board side? The cable around one meter
4. Do we need to swap our TX/RX between up board & down board?
ex: up board TX --> down board RX
up board RX --> down board TX
5. What is fig 11 red circle mean? The normal working rating? or the TRS3122E output swing will between +2.7V~-2.7V??
6. The UART input/output power rate as below red circle??
For now our VL is 3.3v, so the UART power rate will be 3.6v?
Thanks!!