We are facing a overheating problem on max3232. We were using another part of another make earlier and never had a latch up problem . The rest of the hardware is well tested and proved. We switched for cost and availability reasons. Can someone at TI throw some light on this latch up issue. The terminals at both end are complementary hardware devices and do not use DTR pins etc with only Rx Tx mutually coupled.
It appears to be a silicon defect.