This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TRS3221: May we have IC can support Serial Ports RS-232 / RS-485 (Dual mode / Software Selectable RS-232/RS-485 ports)?

Part Number: TRS3221

Hi Sir 

May we have IC can support as below spec?

  1. Serial Ports RS-232 / RS-485 (Dual mode / Software Selectable RS-232/RS-485 ports)
  2. RS-232è4 pin (TXD/RXD/CTS/RTS)
  3. RS-485èFull Duplex (TXD+/TXD-/RXD+/RXD-)  

                                                                                                                    Bogey

  • Hi Bogey,

    No, we do not have a single device supporting both of these interfaces today. We do have several RS-232 and RS-485 transceiver devices, though, and these can be used together to achieve a software-selectable RS-485/232 interface. For an example implementation, you could reference the following design:

    www.ti.com/.../TIDA-00540

    I would be interested in hearing more about your application if there are any further details you are willing to share.

    Regards,
    Max