This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

TUSB8041: USB Hub Not Recognized

Part Number: TUSB8041

Hi,

TUSB8041 USB Hub is not recognized when we connecting to PC.

External EEPROM is not populated and having configure as above.

 

SDA         - pin 37 - pullup   - 2.0V

SCL         - pin 38 - pullup   - 2.0V

SMBUS#     - pin 39 - pullup   - 3.3V

 

FULLPWRMGMT - pin 40 - pulldown - 0.0V

PWRCTL_POL - pin 41 - pulldown - 0.0V

GANGED     - pin 42 - pulldown - 0.0V

 

AUTOEN#     - pin 45 - pullup   - 3.3V

Test       - pin 49 - pulldown - 0.0V

 

Pin 48 (VBUS Voltage)           - 499mv

Pin 62 (Clock frequency)       - 12 Mhz

Pin 50 (reset dissertation)     - 10ms

 

Thanks

Jagadeesh

  • Hi Jagadeesh,

    The clock input for the TUSB8041 should be 24 MHz.

    Regards,

    JMMN

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.