Hi,
Assume there's an abnormal type-C device now, the USB HS data (DP or DM) is short to VBUS. When this device is connected to an NB with TPS65982 on it, DP (or DM ) is short to VBUS which is 5V. Considering these DP/DM signals from type-C connector are connected to TPS65982, what will happen to TPS65982? With DP (or DM) are 5V, will TPS65982 HS MUX still operate normally and pass DP/DM signal to USB host controller?
Thanks!
Antony