Other Parts Discussed in Thread: TPS65982
Hello,
I am developing a device and I need to get 15v with at least 2a on the USB-C port as part of the source power profile. I have read many of the documentations I can get my hands on this module and I can't find it. I did find that this device can't output 15v (or 14.8v)
Page: 13 / Section 5.3.3
http://www.ti.com/lit/ug/slvuaf8c/slvuaf8c.pdf
However, one note I read in another document shows a 14.8v PDO as an option, so I am thinking if I can just flash this device with a new firmware to get the 14.8v (or 15v) from this device.
Page 8 / Section 2.3.3
If this is not at all possible, kindly suggest an alternate Evaluation Board module, or how to modify this board to get it to act as source and negotiate the 15v 2a power delivery...