dear Sir
If our application is TypeA to TypeC dongle
And TypeA input have R6 / R7 / R26 / R27 pull down resistor ,is the schematic correct ??
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Kai,
That's correct, you only have to increase the AC caps to 0.5uF (C6, C7, C8, C9, C12, C13). This is because these capacitors will end-up in series with the AC coupling capacitors on the Device and Host. (It is the same design we used on the HD3SS3220 DFP Dongle Evaluation Module).
Regards,
Diego.