Hi team,
I have two questions about update FW by USB memory, please kindly help. Thanks
1. In orderto write SPI ROM by USB memory, it is necessary to set the regions as following?
Region 0 : 0x2000
Region 1 : 0x20000
With reference to TI document “TPS6598x FW Update From Embedded Controller Over I2C”.
[Process]
step1:check Regions address = {0x00002000, 0x00020000} (refer to TI document P12)
const uint32_t rgnPntr1Val[2] = {0x2000, 0x20000};
step2:If step1 is OK, proceed FW writing process, if else issue error.
So to make sure FW update success, we need to ensure to set Regions as 0x2000 & 0x20000? Could we modify the address or even skip this checking process?
2. Does it relate to the low region file? Because we find the regions address may be changed to "Region0:0x2000 Region1:0x12000" in the early Application Customization Tool version.
Thanks