Other Parts Discussed in Thread: TUSB322, HD3SS3220, , TPS2590
Hi!
here's what I need to do:
1. Have a tablet with USB-C as the master. Should control two devices (may or may not be USB-C).
2. One of the above devices will actually have the hub in question laid out on its board, with the 5V power serving as the tablet charger, so the port where the tablet (the host) is plugged should be the charging port at a rate of around 1.5 - 1.8A.
I think TUSB320 is the way to go but since it is really new to me, i would like some insight from more experienced folk.
Best
Mike.