Other Parts Discussed in Thread: TPS65981, TPS25820, TPS25810
Dear,
My customer is evaluating a project for notebook, they want to use 2*TPS65982 in their two type-C ports.
Two ports have different functions, one can support Thunderbolt, DP, Audio while the other don’t have those function.
Here are some questions want to clarify:
-
Since ROM is required in this application, for those two TPS65982, different functions are implemented, can they share one ROM? Besides, do we have any reference design for the two ports TPS65982?
-
For the USB D+/- MUX, does it have redriver or conditioner function? Since the long line trace on the PCB, they are worried about the signal attenuation of D+/D-; Any suggestion for the long trace of D+/D-?
-
For GPIO5~8, if not used, datasheet suggested connect to ground with 1Mohm resistor, can those resistors removed?
Thanks.