This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2556: Thermal question about maximum expected pin and package temperatures

Part Number: TPS2556

Customer is using TPS2556 with a 49.9K current limit programming resistor, thus Ios maximum should be about 2.5A.  Customer would like to know expected package and/or lead temperature when the die is near its 135C thermal shutdown threshold.  They notice the high temperature of the device during a fault condition. 

  • Hi Ronnie,

    Thank you for your question. I have assigned the expert for this device and he should get back to you on Monday.

    Thank you,
    Eric
  • Hi, Ronnie,

    To calculate junction temperature, you can use R-thetaJa as below.

    Tj= Ta+P(dissipation)*R-thetaJa= 135deg+2.5A*2.5A*35mohm*41.5deg/W=135deg+9.08deg=144.08deg.

    To calculate case temperature, you can use Psi Jt.

    Tt=Tj-P(dissipation)*Psi Jt= 144.08deg-0.15deg=143.93deg.

    Regards,
    Bob

  • Bob,

    I understand how to calculate junction and case temperatures based on thermal resistance and/or thermal characteristics and power dissipation.  Before posting my question, I had tried to calculate what the pin and case temperatures might be assuming the device was in current limit and had reached its internal 135C thermal cycling threshold.  However, you need to know what the average power dissipation is to accomplish this calculation.  The peak power dissipation will be high and the junction will hit 135C and the device will shut off until the junction cools by 20C.  What I'm not sure of is how the duty cycle and thermal inertia will impact the overall case and pin temperatures. 

  • Hi, Ronnie,

    Sorry for misunderstanding your question. First of all, I want to confirm the case temperature calculation at current limit condition.
    Tc=Tj-(Vout-Vin)*Ilimit*PsiJT.

    Because part will thermal shutdown when Tj over 135C, so the case temperature's worst case is 135deg. Usually, top(case) dissipation is 5%, pin(lead) dissipation is 40%, bottom dissipation is 55%. PsiJt reflect the thermal relationship between top(case) temperature and junction temperature.

    Regards,
    Bob