This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

High data rate and clock translated

Hi,

I need R G B 10 10 10 bit to be translated from 1.8V to 3.3V and the MAX 165MHz clock to be translated from 1.8V to 3.3V

Please suggest which voltage translator would be appropriate?

  • Hi Hans,
    I would recommend using one of the SN74AVC series of translators, such as the SN74AVC32T245, which is a 32 bit direction controlled translator capable of 380 Mbps data throughput (which should handle your 165 MHz clock).


    Have a question about Logic ICs? Get it answered with our newly updated Logic FAQ page

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.