Hi,
For TXS0108E, when VCCA=1.8v, VCCB=3.3V, the datasheet shows MAX Data Rate is 60Mbps. When used for 50Mbps data rate application, is there anything to take care? Thanks!
regards
david
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
For TXS0108E, when VCCA=1.8v, VCCB=3.3V, the datasheet shows MAX Data Rate is 60Mbps. When used for 50Mbps data rate application, is there anything to take care? Thanks!
regards
david
David,
A few suggestions:
1. Remember that the maximum data specification of 60 Mbps is for translating a push-pull interface, not an open-drain interface.
2. The maximum data rates were tested with the load conditions given in the PMI (Parametric Measurement Information) section of the datasheet.
2. Restrict the trace length as explained in the layout conditions.
Best Regards,
Nirav