Hi,
I'm using SN74AVC4T774-RGY in a design that can have 0V on Vccb during normal operation. My understanding of the datasheet is that partial power down is supported, and the maximum current consumption in this case should be in tens of microamperes. Unfortunately when I measure it I get much large numbers.
My test setup is: DIR1=DIR3=Vcca, DIR2=DIR4=~OE=GND, A1=A3=B2=B4=GND, 100nF bypass capacitors on Vcca and Vccb. All output pins open. No resistors were used.
In case when Vcca=Vccb=3.3V the current consumption is < 1uA
In partial power down:
Vcca = 3.3V, Vccb = 0V current consumption is 5.4 mA
Vccb = 3.3V, Vcca = 0V current consumption is 4.8 mA
Is such high power consumption expected from this device? And is there any way to improve it?
Regards,
Ievgenii Meshcheriakov