Hi
I am using SN74AVC8T245-Q1 part for my application but i am having one doubt if say any data is not transmitting and device is Enabled then will it damage IC.
If so do i need to connect Pull-up or pull-down.
Regards
Nitesh
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
I am using SN74AVC8T245-Q1 part for my application but i am having one doubt if say any data is not transmitting and device is Enabled then will it damage IC.
If so do i need to connect Pull-up or pull-down.
Regards
Nitesh
Hello Nitesh,
I assume that by "not transmitting" you mean that the pins will be floating. If so, that is correct. When the device is enabled you should always have the input pins at a defined state. You can either pull them to ground or to VCC.
Hello Nitesh,
That is correct. You can also pull them to ground. The inputs should always be at a defined state (either VCC or ground) when the device is enabled and no transmission is happening. The outputs can be left floating. For more information about why floating inputs should be avoided you can refer to this app note , Implications of Slow or Floating CMOS Inputs: