Other Parts Discussed in Thread: LSF0101, LSF0102
using lsf0108 to translate 1.8v fpga I/o to 3.3 I/o. is it ok to use 1k pull up on each side. both sides can handle the 3.3ma and 1.8 ma current required. is 1k to big to use on the 1.8v side.
also
lsf0108 ibis doss not allow selecting it as an output for hyperlynx simulation and lsf0101 and lsf0102 ibis models report errors when trying to assign them to simulation
I see the lack of output for the 108 has been asked before in the forum, but I do not see anyone following it up with a response
thanks
error for 102
C:\hyperlynx91\9.1HL\SDD_HOME\hyperlynx64\Libs\lsf0102.ibs:
Warning : at line 82 in file C:/hyperlynx91/9.1HL/SDD_HOME/hyperlynx64/Libs/lsf0102.ibs : Only the first combination from the [Series Switch Groups] will be used.
Warning : at line 123 in file C:/hyperlynx91/9.1HL/SDD_HOME/hyperlynx64/Libs/lsf0102.ibs : Only the first combination from the [Series Switch Groups] will be used.
Error : at line 4109 in file C:/hyperlynx91/9.1HL/SDD_HOME/hyperlynx64/Libs/lsf0102.ibs : Pin model LSF0101_IO_S used by the series pin mapping from pin 4 to pin 5 of component LSF0102DCU does not exist in this file.
Error : at line 4109 in file C:/hyperlynx91/9.1HL/SDD_HOME/hyperlynx64/Libs/lsf0102.ibs : Pin model LSF0101_IO_S used by the series pin mapping from pin 3 to pin 6 of component LSF0102DCU does not exist in this file.
Error : at line 4109 in file C:/hyperlynx91/9.1HL/SDD_HOME/hyperlynx64/Libs/lsf0102.ibs : Pin model LSF0101_IO_S used by the series pin mapping from pin 4 to pin 5 of component LSF0102DCT does not exist in this file.
Error : at line 4109 in file C:/hyperlynx91/9.1HL/SDD_HOME/hyperlynx64/Libs/lsf0102.ibs : Pin model LSF0101_IO_S used by the series pin mapping from pin 3 to pin 6 of component LSF0102DCT does not exist in this file.
Error : Parse failed on file C:/hyperlynx91/9.1HL/SDD_HOME/hyperlynx64/Libs/lsf0102.ibs.
error for 101
C:\hyperlynx91\9.1HL\SDD_HOME\hyperlynx64\Libs\lsf0101.ibs:
Warning : at line 82 in file C:/hyperlynx91/9.1HL/SDD_HOME/hyperlynx64/Libs/lsf0101.ibs : Only the first combination from the [Series Switch Groups] will be used.
Error : at line 4067 in file C:/hyperlynx91/9.1HL/SDD_HOME/hyperlynx64/Libs/lsf0101.ibs : Pin model LSF0101_IO_S used by the series pin mapping from pin 3 to pin 4 of component LSF0101 does not exist in this file.
not output option for 108
Error : Parse failed on file C:/hyperlynx91/9.1HL/SDD_HOME/hyperlynx64/Libs/lsf0101.ibs.