Other Parts Discussed in Thread: SN74AVC4T774, TXB0104
Loking for similar translator to the LSF0204 but for unidrectional
the current one (bidirectional) makes problems.(it has high output impedance)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello eli,
I think the SN74AVC4T774 would be a good fit. It has individual direction control pins to configure the lines for your signals and can translate between 3.3V and 1.8V. It is only available in PW, RSV, and RGY packages though.
The TXB0104 is available in the RUT package and could also work.
What data rate are you operating at? Are you going to be driving over long traces or cables?