Dear Team,
I have grounded unused inputs of SN74LVCH16T245, Is it ok right?
Regards,
Prasanna
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Team,
I have grounded unused inputs of SN74LVCH16T245, Is it ok right?
Regards,
Prasanna
Hi Prasanna,
Since each channel of the SN74LVCH16T245 can change direction, I would usually recommend grounding all unused inputs and outputs through large resistors (10kΩ or larger). The resistors will limit current in the event that an output doesn't drive all the way to ground, and will keep all unused inputs from floating.
If you have configured the device as unidirectional (ie if the DIR pins are permanently set high or low), then you can directly connect the inputs to ground and leave the outputs floating.