Other Parts Discussed in Thread: SN74LV1T34, SN74LVC1G17
I’m trying to use the voltage translator TXB0108 in order to activate a relay (green dotted box) with a microcontroller through this voltage translator (blue dotted box). The connection between the two regions is done using flat IDC cable.
The circuit in the green box works really fine by itself, and also the circuit in the blue zone works good. Perhaps, I have some problems when interfacing both circuits, which we though are related to impedance mismatching and/or due to capacitance of the IDC cable.
Our idea is to activate a relay and afterwards, we would like to read its state through voltage divider (R2 and R4).
Well, when interfacing the circuit, we could activate the relay, perhaps we are not capable to switch correctly the “ACTIVATION FROM MICROCONTROLLER” node, but we can’t read the high value in “MICROCONTROLLER READING” node.
We did several tests with capacitors in series/parallel with R2 and/or R4 but we didn’t find the solution.
Maybe a solution could be using TXS0108 but we are not sure.
It would be really helpful to receive some help. Thanks in advance.