Hi, Every one.
I have a question on LSF series.
By the datasheet, "External driver must be able sink current on both side"
And Example of the datasheet was 3mA, 10mA, 15mA...
But my external driver device's maximum sink current is 1.6 mA
According to the datasheet, I must select pull-up resister for 0.8mA.
I think 0.8mA is so low value from 3mA~15mA.
I wonder mimimum current of LSF series or maximum pull-up resister.
I can design 0.8mA, or 0.1 mA by using LSF series?
And How does this affect the speed of the signal?
Thank you.