Other Parts Discussed in Thread: AM3354
Hi,
My customer is considering to use TXS0206A device. But its use case is not level shifter.
In my customer's system, the distance from the host processor(AM3354) to SD card is long. It exceeds the limitation of the wiring restriction of SD standard.
My questions are below.
1) So customer would like to extend the distance by inserting TXS0206A between the host processor and SD card. Regarding the power supply, customer use 3.3 V for both VCCA and VCCB. Maximum clock is 55MHz. So SD card bus speed is until high speed. Is there any problem with this use case?
2) According to datasheet of TXS0206A, it is written in the below.
The SDIO lines comprise a semi-buffered auto-direction-sensing based translator architecture that does not require a direction-control signal to control the direction of data flow of the A to B ports (or from B to A ports).
Is this mean that host processor does not need to control the signal direction?
Please advise me.
I appreciate your quick reply.
Best regards,
Michi