This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXS0108E: TXS0108E output issue - output pins not consistent in level shifting

Part Number: TXS0108E

Im having a strange issue with TXS0108EPWR 

I do have a following sonncetion of the mentioned part:

The strange thing is, that on pins A4 and A6 Im having the proper 3v3 -> 5v output, but on the A5 the inout (checked) is the same as for A4 and A6, but the output on the B side is 0.3V for high and goes below 0V for low with - see the following image (taking about the last line)

First line of image is proper B output on A4, second line is the input for A5 and third line is the output for B5

The connection is absolutely the same. I have also replaced the TXS0108E and the result is the same. 

Any ideas? Leads? How to debug this situation? 

Thanks, 

Marcel