Hi Team,
We are evaluating SN74AVC4T774RSVR at the following conditions.
Case1: VCCB pin is 0V but if we input the 25MHz signal to B1 pin, VCCB becomes 2.5V.
Case2: VCCB pin is 0V if we input the low signal to B1 pin.
So, we guess that the voltage of B1 pin appears to VCCB pin.
Is this behavior right?
Regards,
Kanemaru