Other Parts Discussed in Thread: LSF-EVM
Hi,
We need a 6-bit level shifter to support quad mode SPI between AMD CPU (CL around 10pF / SPI @ 1.8V) and SPI flash (W25Q256FV with CL around 30pF / SPI @ 3.3V). Among the 6 signals, 4 data signals are bi-directional. CLK and CS signals are uni-directional. The max speed needs to be support is 66.6MHz.
Would LSF0108 be a right solution for this? Or any other part is preferred?
Thanks!
Antony