Hi,
I got my TXB0108 board, it has everything to plug and go. I wanna use it for SPI, to communicate between Arduino Mega, which has 5 v level and nrf51 which has 3.3v level.
So, I used 4 channels. Vcca connected to 3.3v, Vccb connected to 5v. GROUND is common.
Channels 1 to 4 of A side connected to MOSI, MISO, CLK, CS of nrf51, Channels 1 to 4 of B side connected to MOSI, MISO, CLK, CS of Arduino. OE connected to Vcca, other 4 pins of sides A and B are floating and are not connected to anything. I run my program and logic analyzer shows incorriect data, usually that I send FF and receive FF, of course I send another data.
Once when I just got this chip, I could connect sides incorrectly. 5v to side A, 3.3v to side B, also OE to 5v. Could I damage this chip with this configuration? Datasheet says that Vcca <= Vccb, but if Vcca > Vccb it doesn't damage the board. However, Vcca power supply must be up to 3.6v