I'm trying to experiment with CD4504B part to level translate from 3.3V to 15V.
The Vcc and inputs signals to the CD4504B come from a '28069M DSP (5V &3.3V respectively).
The Vdd for the CD4504B will be 15V from a SMPS.
1. Is there a better part available to accomplish 3.3V to 15V level translation which can fit to F28069M?
2. Is there an issue or limitation with the CD4504B that i should be aware, as its very old IC family.
3. What will the approximate output current using these voltage translations.
Thanks,
Rishi