This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXS0108E: VOHA and VOHB

Part Number: TXS0108E

Hi all

Would you mind if we ask TXS0108E?

We have question about VOHA and VOHB.
The datasheet shows "VCCA × 0.67".
Does it mean in any case, Outvoltage has to be over "VCCA × 0.67"?
It does not mean that Outvoltage is Vcc*0.67=3.35V, right?
We would like to understand correctly.

Kind regards

Hirotaka Matsumoto

  • Hirotaka san,

    Yes, your understanding is correct. The the min Voh and the max Vol is guaranteed as mentioned in the datasheet to account for the process, temperature variations.
    Normally, the voh would be about 0.9Vcc under typical operating conditions.