This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LSF0102: 100MHz signal communication

Part Number: LSF0102

Hello,

LSF0102 has 100MHz communication ability. When both drivers are push-pull and driving 50ohm strip line capability. 

It is needed the translation between 1.2V and 1.8V. The signal bandwidth is 100MHz.

Can LSF0102 use as level translator in this case? If yes, how do we determine pull-up resisters?

Best regards,

Toshihiro Watanabe

  • Hi Toshihiro,

    I am linking one of our Logic Minute videos for this device that should help answer both questions at the same time.  I recommend watching the whole video, but the 4 minute mark is what you are looking for. There are several other videos you can watch that will help you better understand the LSF device as well.