ISO1541: Does TI has 25MHz bi-directional digital isolater like ISO1541?

Part Number: ISO1541

Hi Team,

Does TI has 25MHz bi-directional digital isolater like ISO1541?

If not, are we going to have one in near future?

Thanks.

Andrew

1 Reply

  • The fastest I²C speed is Ultra-Fast Mode at 5 MHz.

    For what application is this? Are you really sure that you need bidirectional signals (i.e., both directions on the same signal line), as opposed as two unidirectional signals in opposite directions (as in, e.g., the ISO7321C)?