• TI thinks resolved

ISO7320-Q1: Superior EMC characteristics

Part Number: ISO7320-Q1

Hi

Our customer evaluates ISO7320-Q1 and ISO7321-Q1 for EMC, as a result, these devices offered superior EMC characteristics compared with competitors.

Could you confirm following requests?

- Can you share EMC evaluation result if any?

- Why does these devices offer good at EMC robustness?  Can you tell us your expertise?

BestRegards

  • Hi,

    Thank you for acknowledging the EMC improvements on the ISO732x devices.

    Could you please share some additional details on the testing that was done?
    Which kind of test/ which standard test was done during the evaluation? I can help with details accordingly.

    Regards,
    Anand Reghunathan
  • In reply to Anand Reghunathan:

    Hi Anand

    Thank you for your reply.
    According to the customer, it is emission test based CISPR25.

    Do you have information to be shared?

    BestRegards
  • In reply to na na78:

    Hi,

    Unfortunately I don't have the CISPR25 data for ISO73xx devices. I've included the CISPR25 data for ISO77xx device below.
    ISO77xx family of devices are superior in isolation and EMC/EMI performance as compared to ISO73xx devices. I would recommend that customer use ISO77xx device in place of ISO73xx device.
    Please do let me know if customer is ok with this data.

    Regards,
    Anand Reghunathan

    ISO774x_CISPR25_E2E.pdf