• Resolved

ISOW7842: Do you anticipate a version of ISOW7842 w/ 5.7K Isolation Rating , 8K Surge Rating and 60601-1 Certification? If so, when?

Part Number: ISOW7842


  • Hi Jon,

    ISOW784x should already be 60601 certified.
    Regarding the other parameters, we usually don't see a request for this level of isolation rating.
    Could you please give me an idea of the end application the device will go in?

    Anand Reghunathan
  • In reply to Anand Reghunathan:

    Hi Anand,

    Thanks for you fast reply.

    I'd like to use the ISOW784x in a medical application.

    Are both the data lines and power isolation sections of this part suitable for a medical device that draws power from a USB port?

    If not, is there another part in development that is more suitable?



  • In reply to JonP:

    Hi Jon,

    Anand is out of office for a few days so I thought I would comment in the mean time. Yes, ISOW78xx is suitable for medical application. We've had customers use this part in a medical application before.

    Best regards,
  • In reply to Dan Kisling:

    Hi Jon,

    It's been about a week since we've heard from you, so I'm going to assume we have resolved your question about ISOW78xx certifications and ratings. If that is correct, feel free to click "This resolved my issue." If we have not resolved your question, please respond to this thread or create a new thread.

    Best regards,