This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

ISO35: Isolation Rating

Part Number: ISO35

Hi Team,

If ISO35 can support max 3000 Vrms Isolation Rating?  Although I found it is only 2500Vrms in datasheet...

If not, do we have any other P2P device can support 3000Vrms Isolation Rating ?

 

Thank you.

  • Hi Lilian,

    Thanks for posting your question on E2E. We do not currently have an isolated RS-485 transceiver that supports 3kVrms Isolation. You are correct that the ISO35 datasheet specification for isolation is 2500 Vrms as per UL 1577 and CSA CA5A and IEC 60950-1. I do not have any pin-to-pin compatible solutions for you at this time.

    To meet 3kVrms Isolation, I would recommend an isolator + RS-485 transceiver such as the ISO7741 + SN65HVD1473. If you also need isolated power, consider ISOW7841 + SN65HVD1473 which can be seen in the Isolated RS-485 With Integrated Signal and Power

    Reference Design. Both of these solutions would give you at least 5kVrms isolation.

    Let me know if that answers your question!

    Best regards, 

    Dan

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.