This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

ISO7763: Low-Frequency PWM signal

Part Number: ISO7763

Dear All,

our customer would like to use the ISO7763 for isolating a PWM motor control signal.

It is expected to have a signal of some kHz with high and low duty cycle. Will the ISO7763 have any problems with that?

I do not think so, as the d/s states that it could be used from '0Mbps' on.

But kindly asking to confirm.

Thanks and best regards
Martin

Does this post answer Your question? Please mark it with the "Verify Answer" button.

  • Hi Martin,

    For ISO7763, the datarate can be anywhere from DC to 100Mbps with any duty cycle provided the pulse width of signal is > 10ns. Thanks.


    Regards,
    Koteshwar Rao

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.