This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO3086: Question about pin1, 2 of ISO3086 chip

Part Number: ISO3086

If the pi1,2 is NC, the ISO3086 chipset can do normal operation?

VCC1, VCC2 is connected to each 3.3v and 5V, They are isolated DC powers.