This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN6505B: Current limit of SN650x

Part Number: SN6505B

Hi guys, 

Is there a way of changing the current limit of SN6505 to a lower one? 

but, not as low as SN6501. Customer needs a current limit around 0.9A typ and 1.1A max.

Regards,

Jon

1 Reply

  • Hi Jon,

    Currently this feature is not implemented as is in SN6505.
    An external current limiting circuit will be required to implement this required limit.

    Regards,
    Anand Reghunathan

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.