Other Parts Discussed in Thread: ISO1540
Section 8.4 suggests that Port 1 has precedence but that isn't stated specifically. Can the master be on Port 2 or will that possibly allow Port 1 to load the SDA2 line?
Is the ISO1541 designed to be placed between an I2C Master and an Isolated bus, or can it be placed between an I2C bus and an isolated I2C slave? I ask because Port 2 can handle much more parasitic capacitance (400 pF) than Port 1 (40 pF), so a bus on Port 1 doesn't make sense.
Thanks,