A customer I support wants to use the ISO7841FDWW for isolation of an SPI link between a DSP and an ARM processor.
The norm for certification is EN 61010-1:2010 (3rd Ed) up to a working voltage of 1000Vrms.
In the table on page 9 of the datasheet this spec is mentioned under the TUV certification but not under CSA.
According to the line above the table are CSA certifications planned. Does that also applies to the EN 61010-1:2010?