Other Parts Discussed in Thread: ISOW7842, ISO7231M
Hello,
Can the ISOW7841 be used for I2C? If so, is there an example circuit?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I²C uses bidirectional open-drain signals.
The ISOW7842 has two unidirectional push/pull channels in each direction. It would be possible to use it for I²C if you add additional circuitry to convert the signals; see Designing an isolated I²C Bus® interface by using digital isolators (SLYT403).
Hi Mitch,
As Clemens has mentioned, please refer to Designing an isolated I²C Bus® interface by using digital isolators.
According to Figure 5, two digital channels in opposite directions are required to realize one I2C channel.
ISOW7842 (2 forward and 2 reverse channels) would be required to realize two I2C channels.
Regards,
Anand Reghunathan