Other Parts Discussed in Thread: ISO7720, ISO7420
Hi,
Customer has two questions below.
Could you answer me, please?
Q1:How fast is the carrier frequecy of LF side?
Q2:Can you tell me the operation of PWM block of LF side?
I think the same of ISO7720. is it correct?
If my idea correct, How does PWM block detect input logic of High/Low?
Customer has a issue at noise insertion test.
It is that voltage waveform is not same between input and output.
He wants to know to consider this issue.
Signal is about 100bps.
Best regards,
Shimizu