Hi,
I am checking the current consumption of the device.
I saw variations in the current consumption of the data sheet, but there is no MIN data.
Is there data on the following conditions indicated in yellow?
Also, is there data when VCC1 and VCC2 are 3.3V?
Later, the difference between ICC1 and ICC2 is large. Is there a reason? The internal block does not seem to have such a large difference between VCC 1 side and VCC 2 side.
Best Regards,