Is there any power ramp up sequence required in ISO1050? It looks that VCC2(Transceiver-side supply voltage)ramp earlier than VCC1(Digital-side supply voltage). the CAN output does not output (CANH and CANL) in short period. but if zoom out the observe time, the ISO1050 output correctly.
Is that due to ISO1050 device need the time to resume from protected state to normal operation?
Yellow : VCC1_3.3V
Blue : TXD(ISO1050 input)
Purple : VCC2_5V
Green : CNA BUS(CANH-CANL; ISO1050 output)
Longer the time, the CAN looks working well.