Dears:
Could you kindly help to check some issues about VCC2?
From datasheet we can see the num of VCC2 is 4.75-5.25V, and the Max num is from -0.5 to +6V.
And the design condition as follows:
1,we use the power module(5V-5V-1W) to power VCC2 of ISO1050DUB.
2,The output voltage of power module will be influenced by the power consumption of IOS1050DUB.
If the current is lower than 20mA, the output of power module is higher than 5.25V or 5.35V, and even 5.5V.
But the output voltage will not exceed to 6V.
Based on the design conditions, we need to confirm the below issues:
1, Whether will it damage ISO1050DUB if the VCC2 is higher than 5.25V and lower than 6V, and is there any influence about the performance of ISO1050DUB?
2, Is there any zero power consumption of situation about ISO1050DUB except for no power?
3, Do you have the test result or graph of power consumption from power on to keep working?
Pls. kindly help us!
Thanks!
Best regards
Luck Wu